What’s this tag on my strainer?
If you just purchased a new strainer, you’re probably wondering about the two pressure sensors at the inlet and outlet of the strainer. THEY’VE BEEN PRE-INSTALLED! These sensors, when connected, monitor the pressure drop that occurs over time when a strainer screen becomes clogged by foreign particles. When the differential pressure across the strainer screen exceeds the pre-configured threshold, an alert is triggered informing that action is required.
The sensor remains off and does not transmit data until activated and connected via an add-on Connection Kit (sold separately). The addition of the sensor to your strainer does not change its certification, function, or specification.
Reliable Alerts, Your Way.
Choose the Connection Kit that’s right for you. Alerts you can count on are just a few easy steps away via a wired or cellular connection with Syncta, the mobile app from Watts or your BAS/BMS.
Why Connect?
Talk to any facility manager and they’ll tell you that maximizing system uptime and protecting critical process equipment from damage is a top priority. With smart and connected differential pressure monitoring enabled on your duplex or wye strainer, you can perform system maintenance proactively rather than reactively.
Maintain Consistent Flow and Efficient System Performance
Proactively Perform
Strainer Maintenance
Prevent Costly
Property Damage
Add Differential Pressure Monitoring to Any Install
Ready to connect? Your new strainer arrives with a connection-capable sensor. This sensor is turned on with the purchase of an add-on Connection Kit. Once you’ve purchased, installed, and activated your Connection Kit, you’ll receive real-time alerts that keep you ahead of slow performance, damaged equipment, and production downtime.
How it Works
Frequently Asked Questions
-
Can I upgrade any existing strainer with SentryPlus Alert smart strainer technology?
-
Does my new strainer include smart sensors?
-
Does my strainer with sensor need a Connection Kit to work?
-
Where does my data go?
-
How do I set up my Syncta profile?
-
Who do I contact for technical support?
-
Can I use smart strainer technology on my Watts Wye Strainer?
-
Can the Sensor Control Module be installed outdoors?
Select Your Connection Kit to Activate your Strainer
Activated through these add-on Connection Kits, the sensor can trigger the alert system sending notification of a change in pressure to facility personnel.
Kit: STR-BMS-Class 150
692MFDB SM
791MFAH SM
792MFDH SM
792MFHH SM
Kit: STR-BMS-Class 150
758CI-N SM
Kit: STR-BMS-Class 600
794MFHH SM
Kit: STR-BMS-Class 600
752CI-N SM
758G-DI SM
Kit: STR-CELL-Class 150
692MFDB SM
791MFAH SM
792MFDH SM
792MFHH SM
Kit: STR-CELL-Class 150
758CI-N SM
Kit: STR-CELL-Class 600
794MFHH SM
Kit: STR-CELL-Class 600
752CI-N SM
758G-DI SM
Kit: STR-SENSOR RPL-Class 150
692MFDB SM
791MFAH SM
792MFDH SM
792MFHH SM
Kit: STR-SENSOR RPL-Class 150
758CI-N SM
Kit: STR-SENSOR RPL-Class 600
794MFHH SM
Kit: STR-SENSOR RPL-Class 600
752CI-N SM
758G-DI SM
Kit: STR-CELL UPGRADE KIT
692MFDB SM
791MFAH SM
792MFDH SM
792MFHH SM
794MFDH SM
794MFHH SM
Kit: STR-CELL UPGRADE KIT
752CI-N SM
758CI SM
758CI-N SM
758G-DI SM
Want to learn more? Need support? We’re here to help.
Fill out this form and your local rep will reach out.